S32K3 LPCMP module propagation delay issues of Trigger mode?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3 LPCMP module propagation delay issues of Trigger mode?

1,172件の閲覧回数
zhanguiyang
Contributor I

zhanguiyang_0-1683433152098.png

When NSAM=0, is this the location where sampling occurs?

If that's the case, I think it's unreasonable because the sampling value at this point is not the result of the selected channel 1.

0 件の賞賛
返信
2 返答(返信)

1,124件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @zhanguiyang,

It is under an internal discussion,

I will update the thread as soon as possible,

 

Regards,
Daniel

0 件の賞賛
返信

1,048件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @zhanguiyang,

It has been confirmed by the design team that NSAM can be set to 0 in this mode.

The sampling can start at the time the channel is selected.

 

Regards,

Daniel

0 件の賞賛
返信