S32K3 LIN

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K3 LIN

2,094 次查看
Chenxu1
Contributor II

Hi,NXP experts;
We are using S32K310 for a lighting project with Lin bus.
For MCU parameters and protocol accuracy, please fill in the following form. We can't get some data from the manual, so please help to improve it.
Thank you!

Oscillator for microcontroller 1

Answer

Supplier explanations

Type

RC

Built-in crystal oscillator

Manufacturer

NXP

 

Part name

S32K310NHT0MLFST

 

Frequency fOSC [MHz]

48MHz

 

Temperature range [°C]

-40 +150

 

Fundamental tolerance (∆fINIT) [%]

  

Temperature tolerance (∆fTEMP) [%]

  

Aging tolerance (∆fAGE[15 years]) [%]

  

∆fSUM = ∆fINIT + ∆fTEMP + ∆fAGE[15 years] [%]

  

LIN microcontroller (baud rate synchronization)

Answer

Supplier explanations

Is baud rate synchronization used?

yes

 

Length of the counter register within the microcontroller [bits]

32

 

Number of measured bits from the Sync byte field

  

Counter frequency [MHz]

  

Integrated oscillator trimming?

  

Minimum baud rate of the synchronization range [bit/s]

1000

 

Maximum baud rate of the synchronization range [bit/s]

20000

 

Error in measurement [%]

  

Error in calculation [%]

  

Error in setting [%]

  

Baud rate tolerance

Answer

Supplier explanations

Maximum baud rate tolerance [%]

0 项奖励
回复
2 回复数

2,069 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

datasheet specifies FIRC Frequency deviation FIRCacc across PVT (process, voltage, and temperature) after trimming. Aging would be included into specified +-5%

RM's LPUART chapters 77.3.5.1 Data sampling technique, 77.3.2 Baud rate tolerance and 77.3.3 Calculating baud rate tolerance would help to gather other parameters.

Nothing more is available.

BR, Petr

0 项奖励
回复

2,042 次查看
Chenxu1
Contributor II

OK,Thanks for your reply。

0 项奖励
回复