s32k312 advanced secure boot can run

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32k312 advanced secure boot can run

Jump to solution
739 Views
victory
Contributor V

Hi NXP,

   i am working on advanced secure boot.  sucessfully write smr and cr.  in jlink debug mode, it can run, but without jlink, run from power on,  it can' t run successfully, (uart  no ouput). could you give me some advice what's i am missing?

 

------------------------

here is my output in debug mode.

s32k configure project v1.5 .............15:13:03
reason 1, 1
uid1:
00| 1F 1C 02 97 65 03 09 23
> 55A5AA33, fw: 2.40.0
> 55A5AA33, lifeCycle: 4
capabilities: 55a5aa33
00| B7 BF FF FC 01 00 00 00
>55a5aa33 ADKPm 1, startuser 0
>55a5aa33, adkp:
00| A7 C7 83 12 25 9C 80 C7 11 22 94 F0 B3 74 71 48
> 55a5aa33 debug auth mode: 1
>55a5aa33 ivt auth: 0
> HSE_STATUS_RNG_INIT_OK
> HSE_STATUS_HOST_DEBUGGER_ACTIVE
> HSE_STATUS_INIT_OK
> HSE_STATUS_INSTALL_OK
> HSE_STATUS_BOOT_OK
> HSE_STATUS_CUST_SUPER_USER
get boot status: 55A5AA33
smr verify: 00000001 00000001
core boot: 00000001 00000001
install: 00000001
cstack used 15%

Tags (1)
0 Kudos
Reply
1 Solution
714 Views
victory
Contributor V

sorry , not hse problem. fixed.

View solution in original post

0 Kudos
Reply
1 Reply
715 Views
victory
Contributor V

sorry , not hse problem. fixed.

0 Kudos
Reply