S32K3 LCU Two-channel multiplexer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 LCU Two-channel multiplexer

Jump to solution
2,636 Views
wuxianlong
Senior Contributor I

Hi,friends

When I was learning LCU, I met a problem and I hope to get your help.
As i see it .
In Logic diagram ,if Sel = 0 ,Y == A. if Sel = 1, Y == B.
But,In Waveforms , when Sel = 1, Y  !=  B. Why ?

企业微信截图_16569868003868.png企业微信截图_16569870872036.png

Tags (1)
0 Kudos
Reply
1 Solution
2,627 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

it is explained in the last sentence of the Waveforms chapter...

Writes to SWEN and SWVALUE have immediate impact on LC outputs, whereas LC inputs require input synchronization to prevent metastability.

Synchronization is 2 LCU clocks as mentioned in the figure 257. So Y has value of A or B delayed by 2 clocks. SEL value also takes effect after 2 clocks while SWEN and SWVALUE immediately.

PetrS_0-1657188291302.png

BR, Petr

View solution in original post

0 Kudos
Reply
2 Replies
2,628 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

it is explained in the last sentence of the Waveforms chapter...

Writes to SWEN and SWVALUE have immediate impact on LC outputs, whereas LC inputs require input synchronization to prevent metastability.

Synchronization is 2 LCU clocks as mentioned in the figure 257. So Y has value of A or B delayed by 2 clocks. SEL value also takes effect after 2 clocks while SWEN and SWVALUE immediately.

PetrS_0-1657188291302.png

BR, Petr

0 Kudos
Reply
2,619 Views
wuxianlong
Senior Contributor I

Hi, PetrS

Thank you for your help.

 

BR,

0 Kudos
Reply