S32K3 HSE Demo project compile error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 HSE Demo project compile error

Jump to solution
895 Views
Temple
Contributor I

image.png

After decompressing the official project, there is a compilation error.

How should I do?

0 Kudos
Reply
1 Solution
858 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

This is an outdated example based on S32K3_RTD_1_0_0_HF01_D2111. You need to use S32DS.3.4 with S32K3 Real Time Drivers Version 1.0.0 HotFix 01 installed to compile it.
Considering that you are a Chinese customer, it is recommended to ask Distributor FAE for the latest s32k3_hse_lib_rtd400hf01_20250221.7z which contains the project for installing HSE FW for S32K312.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
859 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

This is an outdated example based on S32K3_RTD_1_0_0_HF01_D2111. You need to use S32DS.3.4 with S32K3 Real Time Drivers Version 1.0.0 HotFix 01 installed to compile it.
Considering that you are a Chinese customer, it is recommended to ask Distributor FAE for the latest s32k3_hse_lib_rtd400hf01_20250221.7z which contains the project for installing HSE FW for S32K312.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply