S32K3 Flexcan FIFO MB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3 Flexcan FIFO MB

1,829件の閲覧回数
Jon123
Contributor II

Page 38 of RTD_CAN_43_FLEXCAN_UM.pdf:

*****************************************

3.6.3 Legacy Rx FIFO Configuration The receive-only FIFO is enabled for specific controller by
asserting the FEN bit in the MCR register. The Legacy RxFifo configuration in the Tresos plugin is implemented
by selection CanRxFiFo tab to CanLegacyFiFo in CanRxFiFo container.
When the Fifo is enabled, the memory region normally occupied by the first 6 MBs is normally reserved for use of
the Fifo engine. The CPU can read the received frames sequentially, in the order they were received, by repeatedly
accessing the MB0 structure.
The interrupts corresponding to MB0 to 5 have a different behavior when Rx Fifo in enabled. Bit 7 of the IFLAG1
becomes the “Fifo Overflow” flag, bit 6 becomes the “Fifo Warning” flag, bit 5 becomes the “Frame Available in Rx
Fifo” flag and bits 4 to 0 are unused. If Legacy RxFifo is enabled for a specific controller, the user shall configure at
least 1 hardware object which use that controller.

*****************************************

As far as I know, when Legacy RX FIFO is activated, the RAM where the first six standard X mailboxes are located becomes six RX FIFO in depth, and then becomes a Filter table element. Combined with the diagram in the above RTD_CAN_43_FLEXCAN_UM manual and the practical application, it can be seen that only MB0 is being used, so the other five MB's functions are different in the UM manual, but I can't find the specific functions of the other five MB's, that is, M1-M5. Can you answer my doubts? Thank you.

0 件の賞賛
返信
1 返信

1,793件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Jon123

This area is reserved for internal use of the Legacy RX FIFO engine,

Senlent_0-1730709949873.png

 

0 件の賞賛
返信