S32K3 Firmware Update

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 Firmware Update

Jump to solution
2,488 Views
DiaDev
Contributor III

Hello,

Could you please provide the S32K3XX Firmware Update Application Note, similar to the S32K1XX Firmware Updates Application Note (AN12323: S32K1xx Firmware updates – Application Note)?

It would be greatly appreciated!

Thanks !.

1 Solution
2,458 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @DiaDev

There is no direct application note for the S32K3XX devices as with the S32K1XX; However, there are some ANs and examples for FW updates:

Under the S32K3 HSE Demo Examples, there is the Secure boot & Device configuration examples, which showcase basic/advanced secure boot, HSE installation (FULL_MEM & AB SWAP), along with other functionalities.

There is also the OTA DEMO application which can be found in S32K3 Reference Software: SW32K3-REFSW-D.

Finally, you can also refer to the Unified bootloader Demo & the Example S32K312 Bootloader to Application Jump DS3.5 RTD300 from the community.

Hope this helps & best regards,
Julián

 

View solution in original post

0 Kudos
Reply
1 Reply
2,459 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @DiaDev

There is no direct application note for the S32K3XX devices as with the S32K1XX; However, there are some ANs and examples for FW updates:

Under the S32K3 HSE Demo Examples, there is the Secure boot & Device configuration examples, which showcase basic/advanced secure boot, HSE installation (FULL_MEM & AB SWAP), along with other functionalities.

There is also the OTA DEMO application which can be found in S32K3 Reference Software: SW32K3-REFSW-D.

Finally, you can also refer to the Unified bootloader Demo & the Example S32K312 Bootloader to Application Jump DS3.5 RTD300 from the community.

Hope this helps & best regards,
Julián

 

0 Kudos
Reply