S32K3 Cyclic Wakeup and Secure Boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K3 Cyclic Wakeup and Secure Boot

2,694 次查看
Verifono
Contributor I

My requirement is to monitor a sensor while keeping average current consumption < 150 uA. The uC  shortly powers up the sensor every second and reads the sensor's binary value on a digital input. This can be solved with a cyclic wakeup from Standby mode.
My current understanding is that a normal boot sequence is performed on standby exit, which includes secure boot. The measurement could be finished in microseconds, but secure boot extends the Run mode to many millisecods so that the average current is too high.
- Secure Boot is not necessary after Standby. Can it be bypassed?
- Is there a way to switch-off the cores and peripherals without boot sequence after wakeup?
- Any other solution?

0 项奖励
回复
2 回复数

2,636 次查看
Verifono
Contributor I

This is exactly the hint that I was looking for. Thank you very much!

0 项奖励
回复

2,649 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Secure boot is being skipped after fast standby exit as you can see in the following diagram:

davidtosenovjan_0-1688474222754.pngdavidtosenovjan_0-1688474222754.png

Normal standby exits goes over secure boot sequence. If it is not the key point of your question, please clarify.

 

0 项奖励
回复