S32K3 CAN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 CAN

3,727 Views
abc1258
Contributor I

When configuring the CAN communication of S32K3 series core board, I encountered a problem. I hope you can get help. Thank you. The problem is as follows: CAN send and receive (extended and standard) CAN be tested separately. If CAN accept mailbox is enabled, it will enable the accept mailbox interrupt flag when sending, and directly enter the interrupt. How to solve this problem?

 
0 Kudos
Reply
4 Replies

3,696 Views
abc1258
Contributor I

@Senlent ok,thank you

0 Kudos
Reply

3,706 Views
abc1258
Contributor I

@Senlent Thank you for your reply. The previous problem has been solved. When configuring the initialization of CAN, you can just disable the self-receiving,Now we face a new problem, initialize the receiving function and then do processing in the interrupt, will not recognize my ID number, no matter the ID can enter the interrupt and do data processing

0 Kudos
Reply

3,711 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@abc1258

This should be the same as the FlexCAN module of the S32K1 series, the interrupt of the MB is or operation, so when you send it will also enter the interrupt,you can don't care about it in the interrupt handler.

0 Kudos
Reply

3,701 Views
Senlent
NXP TechSupport
NXP TechSupport
0 Kudos
Reply