S32K3 CAN communication

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 CAN communication

2,270 Views
Voledi
Contributor II

Hi NXP's team, 

i have some problems, I attach the source code below

*My Target

-CAN communication between S32K344 and CAN tool based https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-FlexCAN-Ip-TX-RX-EnhanceRXFIFO-test...

*My hardware and Software

-S32K3x4EVB T172/orQ172 i'm not sure,   S32DS 3.5,  RTD 5.0.0

-I connected CANH, CANL, CAN_GND each togeter between Board and CAN Tool, but no date was be traced

*Can you check if they work on your side, and point out my mistakes?

Tags (1)
0 Kudos
Reply
3 Replies

2,242 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Voledi

S32K3X4-T172 and S32K3X4-Q172 are different, and the CAN transceiver are different.

This demo is based on S32K3X4-Q172, and the transceiver used is TJA1153.

And this demo is based on S32 DS V3.4+ RTD 2.0.0, which is not compatible with the version you are using.

The attached is a routine based on S32K311, you can refer to it, the version is consistent with what you are currently using.

0 Kudos
Reply

2,236 Views
Voledi
Contributor II

Can you identify the exact type of board, I'm confused about this

Voledi_0-1735182782568.jpeg

MCU: P32K344EHVPBS0P55A

0 Kudos
Reply

2,212 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Voledi

According to the information in the picture, the transceiver here should be TJA1153, so there is no problem if you refer to this link, but this is based on S32 DS V3.4 + RTD 2.0.0.

https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-FlexCAN-Ip-TX-RX-EnhanceRXFIFO-test...

 

0 Kudos
Reply