S32K3 ADC Precision

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 ADC Precision

Jump to solution
4,539 Views
WeiC
Contributor I

I was using the ADC standard channel of S32K312 to sample the voltage and found that the maximum difference between the result and the real value can reach 6LSB. I think there may be something wrong with my sampling configuration:

The CORE clock is 120MHz, the sampling clock and calibration clock of ADC is 4, and the sampling time configuration is 255, enabling high-speed mode.

Even if I refer to the configuration on the manual, and the result is similar.

0 Kudos
Reply
1 Solution
4,442 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport
 

In principle there are technology reasons why inputs are different - Because we have many analog inputs for ADC and from some pins the analog path is long, we need to use multiple switches on each analog input. On the precision channels the number of switches is limited so it is recommended for main measurements. Standard channels have more switches in the path.

davidtosenovjan_0-1704362546801.png

 

View solution in original post

0 Kudos
Reply
3 Replies
4,495 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

If you read converted value as 6LSB out of "real value", the it is still in the specification (+/- 6LSB)

davidtosenovjan_0-1703858594201.png

 

0 Kudos
Reply
4,492 Views
WeiC
Contributor I

what is the resolution of standard channel ?  I didn't clearly see the resolution in the manual. What is the difference between an accurate channel and a standard channel?

0 Kudos
Reply
4,443 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport
 

In principle there are technology reasons why inputs are different - Because we have many analog inputs for ADC and from some pins the analog path is long, we need to use multiple switches on each analog input. On the precision channels the number of switches is limited so it is recommended for main measurements. Standard channels have more switches in the path.

davidtosenovjan_0-1704362546801.png

 

0 Kudos
Reply