The FIRCREGOFF bit is used to control an internal regulator used by the FIRC internal circuit. In order to guarantee the operation frequency of the FIRC at voltage levels higher than 3V and inside the specs, this bit has to be 0. Unfortunately, we cannot guarantee a frequency operation when the internal regulator is disabled.
This is clear to me, but still don't answer to my question about precision of FIRC, when regulator is turned off. Do you have some hard data ? Is it 4% or more in whole temperature/voltage range ? Another question is, why would anybody want to turn this regulator off ?
The FIRC trimming error bit is applicable when you trim the operation clock of the FIRC to other than the default (48 MHz) and there is detected an error on the change. It is not applicable if you cannot change the freq.
That means that for S32K144x it's not applicable as FIRC can only have 48MHz. Can you please tell me then, to which microcontroller this flag is applicable ?
Best regards,
Dawid