S32K14x MCAL package

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K14x MCAL package

4,679 Views
ravikrishna
Contributor I

Hi,

In NXP AUTOSAR homepage it is mentioned that S32K14x device has MCAL support. But in the MCAL packages list I couldn't find the S32K14x package. Is the MCAL package available for this device? Can you please share the link.

Labels (1)
Tags (3)
0 Kudos
Reply
2 Replies

3,710 Views
pschenke
Contributor II

Be aware, that you may require even so the CSEC package, that is not part of the MCAL package. You may find it here: https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K14-ACSEC421E (be aware that the installer has a bug and create the plugin of CSEC NOT in folder plugins, but in folder eclipse).

Do you have one package of MCAL for the S32K14x that is complete valid? I'm not sure, which package to be selected. A lot of Bugfixes and parts with only one module (e.g. SPI) are listed on the NXP Website...

0 Kudos
Reply

3,710 Views
jorgesuarez-riv
Contributor II

Following the next link you can find the AUTOSAR 4.2 MCAL for S32K14x:

https://www.nxp.com/support/developer-resources/run-time-software/automotive-software-and-tools/auto... 

0 Kudos
Reply