S32K14x MCAL Sample Application

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K14x MCAL Sample Application

2,357 Views
young_man
Contributor I

Why my S32K1XX_MCAL4_3_RTM_1_0_4 has not SampleApplication files?Where is the bag and could someone  provid the files?I need to configration and integration the CAN & LIN modules then testing them

0 Kudos
Reply
2 Replies

2,317 Views
young_man
Contributor I

no,it‘’s not.That question has solved.

But i have anthor problem need to help for yours!

That is below:

Project: lighting_S32K144_4.2_RTM1.0.1<br>CommonPublishedInformation parameter "SwPatchVersion" default in schema XDM of module "IntegrationFramework_TS_T40D2M10I1R0" does not match module registration in its plugin.xml. Fixed value in schema.

0 Kudos
Reply

2,341 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Yes, that could be. Sample application is usually in basic package like 1.0.0 or 1.0.1.

I can see it in 1.0.1 for MCAL 4.3

petervlna_0-1663572198722.png

 

Best regards,
Peter

0 Kudos
Reply