S32K14X SERIES

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K14X SERIES

4,029 Views
hajianik
Senior Contributor I

Hi,

Just finished downloading  S32K Design Studio and did the demo for blinking the LED.

My concern is that it uses processor expert to do it and I get kind of lost, is there a simple project for blinking

the LED not using processor expert that I can import to design studio  as a base and start building my project upon that?

Thanks ,

Koorosh Hajiani

Labels (1)
0 Kudos
Reply
4 Replies

3,302 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi Koorosh Hajiani, 

In case you have a Matlab license then you can try one of the examples from Model Based Design Toolbox (free of charge). There are examples that covers most of the S32K144 peripherals: IOs, FTM, UART, CAN, SPI, I2C, ADC, CMP etc

Have a look here: https://community.nxp.com/docs/DOC-334170 

Hope it helps!

Daniel

0 Kudos
Reply

3,302 Views
hajianik
Senior Contributor I

Thanks,

I will try it and let you know

0 Kudos
Reply

3,302 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi Koorosh,

what about to try simple "Hello" demo example.

pastedImage_1.png

BR, Petr

0 Kudos
Reply

3,302 Views
hajianik
Senior Contributor I

Yes, that one is much better,  Do you know how do I link the standard libraries (printf,sprint,....etc) link with these projects.

Thanks again,

Koorosh

0 Kudos
Reply