S32K148EVB-Q176 debugging issue !

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K148EVB-Q176 debugging issue !

3,422件の閲覧回数
Saitej
Contributor IV

Hello NXP

Am with S32K148 with IDE S32 Design Studio. While am trying to debug with break points, cursor is not getting stopped at the break point. Observed threads got missed to track.

using on board debugger Open SDA

Please do the needfull.

Console Message:

Task name is Task_10ms
Task name is Task_2ms
Task name is Task_1ms
Number of threads 9 qfThreadInfoIterator: 0
Number of threads 9 qfThreadInfoIterator: 9
Number of threads 9 qfThreadInfoIterator: 0
Number of threads 9 qfThreadInfoIterator: 9
rsp_qThreadExtraInfo - Thread extra info grabbed - result: 5461736B5F31306D73
rsp_qThreadExtraInfo - Thread extra info grabbed - result: 5461736B5F316D73
rsp_qThreadExtraInfo - Thread extra info grabbed - result: 5461736B5F326D73
rsp_qThreadExtraInfo - Thread extra info grabbed - result: 5461736B5F356D73
rsp_qThreadExtraInfo - Thread extra info grabbed - result: 5461736B5F3130306D73
rsp_qThreadExtraInfo - Thread extra info grabbed - result: 49444C45
Number of threads 9 qfThreadInfoIterator: 0
Number of threads 9 qfThreadInfoIterator: 9

タグ(3)
0 件の賞賛
返信
5 返答(返信)

3,398件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

it could be caused by optimizations. I would check if the optimization level is set to 0:

lukaszadrapa_0-1617708487337.png

 

Regards,

Lukas

 

0 件の賞賛
返信

3,391件の閲覧回数
Saitej
Contributor IV

Hello @lukaszadrapa 

Thanks for the response 

Currently we have zero optimisation's, Am able to break it in few trials as it is random.

Saitej_0-1617711737105.png

 

0 件の賞賛
返信

3,364件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

is OS Awareness enabled like this?

lukaszadrapa_0-1617787919041.png

 

And if this doesn't help, is it possible to share the project, so we can try to reproduce the behavior on our side?

Thanks,

Lukas

 

0 件の賞賛
返信

3,350件の閲覧回数
Saitej
Contributor IV

Hello @lukaszadrapa 

Yes, OS awareness is enabled , it not helped us.

It's not possible to send the project , if you guide me will share all the logs with to debug the issue.

0 件の賞賛
返信

3,411件の閲覧回数
Saitej
Contributor IV

any help please

0 件の賞賛
返信