S32K148 MCAL sample project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K148 MCAL sample project

1,827件の閲覧回数
luocan
Contributor I

Hello,

    Now I have a piece of S32K148EVB-Q176, I will develop mcal driver. But there  is not the sample  project for S32K148 in the package of S32K14X_MCAL4_3_RTM_1_0_1, especial not  runS32K148.cmm、autosar_flash_148.gld、autosar_flash_148.icf、autosar_flash_148.ld.

How should we solve the problem? 

0 件の賞賛
返信
2 返答(返信)

1,811件の閲覧回数
hungnguyenphi
NXP Employee
NXP Employee

Hello @luocan ,

Please find it in attached file.

Best regards,

Hung

0 件の賞賛
返信

1,447件の閲覧回数
zaineb01
Contributor I

Hello,

     I have S32K116EVB-Q048, I will develop mcal driver too. and i have the same problem, there  is no sample  project for S32K116 in the package of S32K1XX_MCAL_4.0_RTM_CD01_1.0.5 .

How should I solve the problem? 

@hungnguyenphi 

0 件の賞賛
返信