S32K148: Frequent UART_FRAMING_ERROR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K148: Frequent UART_FRAMING_ERROR

4,565 Views
zitong_zhang
Contributor II

Dear all,

I am having some trouble with the UART module where UART_FRAMING_ERROR occurs very frequently that only 20% of the payload is received successfully.

The project uses freeRTOS and the S32 SDK. A task receives UART packets from another chip (iMX6). The UART packet starts with 0xAE and has a fixed length of 88 bytes (RX_BUFF_LEN). It is sent to S32K148 at 100Hz with a baud rate of 460800.

I have used similar tasks to receive data from other devices before, which worked fine. The code also works when I send data from a Raspberry Pi to an S32K148_EVB (same data format as memtioned above). But when switching to the actual project, LPUART_DRV_GetReceiveStatus frequently returns UART_FRAMING_ERROR (as sample from FreeMaster). As a result, only 20% of the payload is received: a counter increases upon successful reception, and FreeMaster shows this counter only increases by 20 each second, instead of the expected 100Hz.

To add a few points:

1. The S32K148 uses CLK_SRC_SPLL_DIV2 as the clock source, process expert shows an actual baudrate of 465116, which doesn't look ridiculous;

2. I have also tried reducing the baudrate to 115200 with no success;

3. The iMX6 chip seems to receive data from S32K148 OK, at least much more smoothly;

I have inserted part of the code below. I wonder if you could share your thoughts on this issue.

Many thanks!

Zitong

 

LPUART_DRV_ReceiveData(INST_LPUART1, &u8RxBuffer[0], RX_BUFF_LEN);
for (;;) {
    /* poll rx status */
    eRxStat = LPUART_DRV_GetReceiveStatus(INST_LPUART1, &u32BytesLeft);
    if ( eRxStat == STATUS_BUSY ) { /* if rx in progress */
        u16BytesReceived = RX_BUFF_LEN - (uint16_t)u32BytesLeft;
        if ( u16BytesReceived > 0 ) { /* if at least one byte received */
            if (0xAE != u8RxBuffer[0]) { /* if packet header missed */
                /* abort current receive since the packet is incomplete */
                LPUART_DRV_AbortReceivingData(INST_LPUART1);
                /* restart receive after 2ms so that the current packet is flushed */
                vTaskDelay(2);
                LPUART_DRV_ReceiveData(INST_LPUART1, u8RxBuffer, RX_BUFF_LEN);
            }
        }
    } else if ( eRxStat == STATUS_SUCCESS ) { /* if transfer successful */
        /* handle received data */
        /* restart receive */
        LPUART_DRV_ReceiveData(INST_LPUART1, u8RxBuffer, RX_BUFF_LEN);
        vTaskDelay(1);
    } else { /* if error occurs */
        /* restarts receive */
        LPUART_DRV_ReceiveData(INST_LPUART1, u8RxBuffer, RX_BUFF_LEN);
    }
    vTaskDelay(1);
}

 

 

Tags (3)
0 Kudos
Reply
3 Replies

2,458 Views
toipaz
Contributor III

1. The S32K148 uses CLK_SRC_SPLL_DIV2 as the clock source, process expert shows an actual baudrate of 465116, which doesn't look ridiculous;

--> the actual baudrate for 460800 in S32K148 can be updated to 460905 by using SPLLDIV2 Clock 112MHz for LPUART clock.

For this,

 1) SPL_VCO set [ / 1 * 28 ] and output 224 MHz

 2) SPL CLOCK set [ / 2 ] and output 112 MHz

Tags (3)
0 Kudos
Reply

3,336 Views
iysheng
Contributor II

I meet similar problem like you, and I fixed this by set rx pin pull up enable.Maybe you can try this too.

0 Kudos
Reply

4,551 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Zitong,

Since the Framing Error is reported when the received char has 0 where a stop bit should be,

danielmartynek_0-1614349309278.png

I would double check the baudrate.

Can you please scope the signal both from the S32K148 and the iMX6?

Please have a look at Section 53.4.2 Baud rate generation in the RM, rev12.1

Depending on the over sampling ratio, the receiver has an acquisition rate of 4 to 32 samples per bit time.

 

Regards,

Daniel

 

 

 

0 Kudos
Reply