S32K148 FTM with SPLL clock source

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K148 FTM with SPLL clock source

跳至解决方案
2,760 次查看
tomasfrcek
Contributor III

Hello,

I have several FTM modules with various channels and operation modes setup in my project. I use the FTM modules to generate periodic interrupts, read and generate PWM signals. So far, I only supplied  the modules with SOSCDIV1_CLK (SOSC = 8MHz, DIV1 = 8MHz).

My current working setup of the FMT:

  • PCC_FTM2 = 0xC1000000 (PCS = 1 (SOSCDIV1_CLK), CGC = 1 (clock enabled)).
  • FTM2->CLKS = 3 (External clock)
  • FTM2->PS = 7 (divide by 128).

But now I need to generate PWM signals with very high frequency, so I need to connect SPLLDIV1_CLK instead of SOSCDIV1_CLK (SPLL_CLK = 100MHz, DIV1 = 50MHz). I setup the FTM in the following way:

  • PCC_FTM2 = 0xC6000000 (PCS = 6 (SPLLDIV1_CLK), CGC = 1 (clock enabled)).
  • FTM2->CLKS = 3 (External clock)
  • FTM2->PS = 7 (divide by 128).

But after configuring the clock this way, the FTM counter won't even start counting.

SPLL is also configured as system clock source. This is the SPLL configuration in SCG:

  • SPLLCSR = 0x03000001
  • SPLLDIV = 0x00000302
  • SPLLCFG = 0x00090000

Thanks for advice!

Tomas

0 项奖励
回复
1 解答
2,745 次查看
tomasfrcek
Contributor III

Hello, again,

So I've managed to get the FTM running with the SPLLDIV1 clock sourced. The answer is in the reference manual, table 27-8. It says the maximum FTM frequency is governed by SYS_CLK. In my case, the SYS_CLK is 50MHz. Trying to supply the FTM with the same clock value 50MHz in SPLLDIV1_CLK still resulted in FTM not counting. But after dividing the SPLLDIV1_CLK down to 25MHz it finally started to work.

T.

在原帖中查看解决方案

1 回复
2,746 次查看
tomasfrcek
Contributor III

Hello, again,

So I've managed to get the FTM running with the SPLLDIV1 clock sourced. The answer is in the reference manual, table 27-8. It says the maximum FTM frequency is governed by SYS_CLK. In my case, the SYS_CLK is 50MHz. Trying to supply the FTM with the same clock value 50MHz in SPLLDIV1_CLK still resulted in FTM not counting. But after dividing the SPLLDIV1_CLK down to 25MHz it finally started to work.

T.