S32K146 adding multiple config set

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K146 adding multiple config set

1,382件の閲覧回数
shubham_prajapati
Contributor I

Hello,

Please guide on "How to add multiple ConfigSet for a module".

I need to add another ConfigSet for the PWM module with different PWM channels.

shubham_prajapati_0-1635143598753.png

 

There is no option as add configset for PWM module as shown below. 

shubham_prajapati_1-1635143707160.png

Is there any other option or method to add configsets for a module?

Thanks in Advance.

Regards

Shubham

0 件の賞賛
返信
1 返信

1,354件の閲覧回数
hungnguyenphi
NXP Employee
NXP Employee

Hello @shubham_prajapati 

 

As the PWM autosar specification, we cannot have two PwmChannelConfigSet in the configuration.

hungnguyenphi_0-1635302054730.png

 

Regarding the question "Is there any other option or method to add configsets for a module?", could you please try the "Post build Variant" from the below thread:

https://community.nxp.com/t5/S32K/S32k146-MCAL-Variant-handling-at-configuration-container-level/td-...

 

Best regards,

Hung

0 件の賞賛
返信