S32K146 RCM_SRS Register value for SWD reset

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K146 RCM_SRS Register value for SWD reset

跳至解决方案
5,444 次查看
adria
Contributor I

Hello,

When I perform a software reset by calling "SystemSoftwareReset()" I read SW (bit 10) as reset cause int the RCM_SRS register. That is perfect.

But when I perform a reset through SWD from the IDE (S32 Design Studio) I am getting the same reset cause.

Is that the correct behaviour?

I can see there is a bit field in the RCM_SRS register for a reset caused by JTAG, shouldn't this be the one active when the reset is caused by SWD?

Thanks in advance!

Best regards,

Adria

标记 (1)
0 项奖励
回复
1 解答
5,247 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Adria,

Yes, it makes sense.

Please refer to J-Link / J-Trace User Guide

https://www.segger.com/downloads/jlink/UM08001 

7.10    Reset strategies

7.10.2    Strategies for Cortex-M devices

Thanks,

BR, Daniel

在原帖中查看解决方案

0 项奖励
回复
4 回复数
5,247 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Adria,

What debugger are you using?

Have you tried resetting the MCU while running an empty project?

The JTAG flag is set only if the debugger selects a certain IR codes.

pastedImage_1.png

pastedImage_2.png

But the debugger can reset the MCU using external reset pin as well.

BR, Daniel

0 项奖励
回复
5,247 次查看
adria
Contributor I

Hi Daniel,

I am using Segger J-Link. When I perform the reset through the IDE (S32 Design Studio) I get a Software reset, and this bit says:

"Software
Indicates a reset has been caused by software setting of SYSRESETREQ bit in Application Interrupt and
Reset Control Register in the Arm core.
0 Reset not caused by software setting of SYSRESETREQ bit
1 Reset caused by software setting of SYSRESETREQ bit"

Instead, when I use PE Micro Multilink Universal as debugger, I get External Reset Pin, and this bit says:

"External Reset Pin
Indicates a reset has been caused by an active-low level on the external RESET (RESET_b) pin.
0 Reset not caused by external reset pin
1 Reset caused by external reset pin"

This last one (with Multilink debugger) makes more sense for me because the debugger can write on the MCU reset pin and so cause a reset through that pin. But in the case of the J-Link debugger, it just felt weird that a reset cause by a user through the debugger triggers a Software reset, which normally is done programmatically from the code.

The only thing I would like to know if it all makes sense?

Best regards,

Adria

0 项奖励
回复
5,248 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Adria,

Yes, it makes sense.

Please refer to J-Link / J-Trace User Guide

https://www.segger.com/downloads/jlink/UM08001 

7.10    Reset strategies

7.10.2    Strategies for Cortex-M devices

Thanks,

BR, Daniel

0 项奖励
回复
5,247 次查看
adria
Contributor I

Hi Daniel,

Thanks!

Best regards,

Adria

0 项奖励
回复