S32K146 Passive Filter Enable function

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K146 Passive Filter Enable function

1,657件の閲覧回数
kkw
Contributor I

Hi:

    I used PTC15 as GPIO function, set input mode with pulldown register and enable  Passive Filter . Then connect 1 HZ, 1KHZ, 1MHZ, 30 MHZ, 50 MHZ square wave  to PTC15. But PTC 15 can detect high. 

   Will Passive Filter function filter high frenquency? Why PTC15 can detect high level? Is all GPIO has this fucntion? 

0 件の賞賛
返信
1 返信

1,646件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi kkw,

Please refer S32K146_IO_Signal_Description_Input_Multiplexing.xlsx that is attached to the S32K-RM.

S32K-RM.png
In IO Signal Table, column U shows the reset state of PCR_PFE (bit 4) and column V specifies which pin has the PFE bit configurable.
Unfortunately PTC15 does not support this feature.

S32K146_IO_Signal_Description_Input_Multiplexing.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信