S32K146 Package Selection without SDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K146 Package Selection without SDK

ソリューションへジャンプ
2,115件の閲覧回数
bjrajendra
Senior Contributor I

Hello all,

I'm using S32K146 144 Pin.

I'm not using SDK for code generation & Configuring the Chip.

I would like to change the package for S32K146. Kindly suggest a suitable way so as to select the package without using SDK

Thanks in advance,

BJ Rajendranath.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
2,005件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

There is the same header file for each package of S32K146.

So, you should just take care that you are using the pins available on your package.

The pinout can be useful. It is available in the RM rev. 11. in the document S32K146 IO_Signal_Description_Input_Multiplexing.xlsx

I hope it helps.

Best regards,

Diana

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,006件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

There is the same header file for each package of S32K146.

So, you should just take care that you are using the pins available on your package.

The pinout can be useful. It is available in the RM rev. 11. in the document S32K146 IO_Signal_Description_Input_Multiplexing.xlsx

I hope it helps.

Best regards,

Diana

0 件の賞賛
返信