S32K146 Package Selection without SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K146 Package Selection without SDK

Jump to solution
2,116 Views
bjrajendra
Senior Contributor I

Hello all,

I'm using S32K146 144 Pin.

I'm not using SDK for code generation & Configuring the Chip.

I would like to change the package for S32K146. Kindly suggest a suitable way so as to select the package without using SDK

Thanks in advance,

BJ Rajendranath.

Labels (1)
0 Kudos
Reply
1 Solution
2,006 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

There is the same header file for each package of S32K146.

So, you should just take care that you are using the pins available on your package.

The pinout can be useful. It is available in the RM rev. 11. in the document S32K146 IO_Signal_Description_Input_Multiplexing.xlsx

I hope it helps.

Best regards,

Diana

View solution in original post

0 Kudos
Reply
1 Reply
2,007 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

There is the same header file for each package of S32K146.

So, you should just take care that you are using the pins available on your package.

The pinout can be useful. It is available in the RM rev. 11. in the document S32K146 IO_Signal_Description_Input_Multiplexing.xlsx

I hope it helps.

Best regards,

Diana

0 Kudos
Reply