S32K146 LPO clock source select

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K146 LPO clock source select

跳至解决方案
949 次查看
ZhaozhangChen
Contributor I

Hi

    I use the default LPO clock 128Khz in the BootLoader, but I need to use LPO clock 1Khz in the APP, but when I set LPO clock 1Khz when the BootLoader jumps to the APP, it does not take effect.The value of LPOCLKSEL register is 00b. Is there any way to set LPO to 1KHz in app.

ZhaozhangChen_0-1665219450690.pngZhaozhangChen_1-1665219497269.png

 

0 项奖励
回复
1 解答
939 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@ZhaozhangChen

The LPOCLKS register is a write-once register, and is reset only on POR or LVD.

 

please refer to S32K-RM,the chapter 11.3.1.4

Senlent_0-1665281155921.png

BR!

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
940 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@ZhaozhangChen

The LPOCLKS register is a write-once register, and is reset only on POR or LVD.

 

please refer to S32K-RM,the chapter 11.3.1.4

Senlent_0-1665281155921.png

BR!

 

0 项奖励
回复