HI,all
I use Flexcan demo, in FLEXCAN_DRV_Init
enable canfd fail,I find FRZ is 1 Freeze Enable,but mcr fden not be set 1.
I want to know why this is happening.
My English is not good. Thank you!
解決済! 解決策の投稿を見る。
Hi,
try to change FDEN within debugger directly, while in Freeze mode.And check part number if CAN FD is even implemented.
BR, Petr
元の投稿で解決策を見る
FDEN can be set in Freeze mode only so do you have FRZACK set as well to indicate module is in Freeze mode? Also consider if CAN FD is available for used module, it is not on FlexCAN2 of S32K146.
Both FRZACK and FRZ are set 1,but FDEN still cannot be set 1