S32K146 Adc Channel configurations array with hw trigger

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K146 Adc Channel configurations array with hw trigger

2,115 次查看
Micha4566465
Contributor II

Hello,

I create an ADC channel configurations array with PDB trigger-hardware.

But I get only an interrupt for (ControlChanIdx == 0).

I configured the system completely in RTD as you can see in the pictures.

Can you help me why there is no interrupt for (ControlChanIdx == 1)?

 

My source code:

// Interrupt routine

void AdcConversionCompleteNotif(const uint8 ControlChanIdx)

{

data = Adc_Ip_GetConvData(ADCHWUNIT_0_INSTANCE, ControlChanIdx);

}

 

int main(void)

{

Adc_Ip_StatusType adcStatus;

Adc_Ip_Init(ADCHWUNIT_0_INSTANCE, &AdcHwUnit_0);

 

adcStatus = Adc_Ip_DoCalibration(ADCHWUNIT_0_INSTANCE);

while (adcStatus != ADC_IP_STATUS_SUCCESS)

{

adcStatus = Adc_Ip_DoCalibration(ADCHWUNIT_0_INSTANCE);

}

 

Pdb_Adc_Ip_Init(PDBHWUNIT_0_INSTANCE, &PdbHwUnit_0);

Pdb_Adc_Ip_SwTrigger(PDBHWUNIT_0_INSTANCE);

 

while (1);

}

标记 (4)
0 项奖励
回复
1 回复

2,078 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@Micha4566465

This problem seems to be caused by setting the delay time of the two trigger channels to be the same.

You can try setting different delay parameters for the two pre-trigger channels.

Senlent_0-1744703480586.png

 

0 项奖励
回复