S32K144EVB UART 8bit Send Receive Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144EVB UART 8bit Send Receive Problem

2,672 Views
hjinha
Contributor II

I use two S32K144EVB for UART Communication.

One only sends value (I will call TX S32K),

the other only receives value(I will call RX S32K).

The problem is that "RX S32K" Can not receive the value over 0x80 ~ 0xFF.

It seems only receive 0x7F(7bit).

"RX S32K" Can receive the value from 0 to 127(0x7F).

Also I couldn't find the value over 0x80 in RxBuff, when using Debug breakpoint.

I  use this function

void LPUART1_transmit_char(char send)

{ /* Function to Transmit single Char */
   while((LPUART1->STAT & LPUART_STAT_TDRE_MASK)>>LPUART_STAT_TDRE_SHIFT==0);
/* Wait for transmit buffer to be empty */
   LPUART1->DATA=send; /* Send data */
}

I try many things, but i don'y know reason about this problem.

Tags (2)
2 Replies

2,501 Views
hjinha
Contributor II

Thank you.

I solved the problem!

The data type was a problem. 

I changed Char data type to unsigned Char data type

void LPUART1_transmit_char(char send)

{ /* Function to Transmit single Char */
   while((LPUART1->STAT & LPUART_STAT_TDRE_MASK)>>LPUART_STAT_TDRE_SHIFT==0);
/* Wait for transmit buffer to be empty */
   LPUART1->DATA=send; /* Send data */
}

2,501 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

Have you analyzed the signal on the bus? 

Is TX MCU sending correct data?

Thanks.

Daniel 

0 Kudos
Reply