S32K144 interface voltage for ISELED

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K144 interface voltage for ISELED

跳至解决方案
3,182 次查看
nanjun
Contributor III

Hello,

the S32K144 is connected to iseledstrip through an adapter board.

The voltage from MCU is 3.3V while LED strip requires 5V. Could the MCU be damaged during read function?

See ISELED ADK User Manual.

Kind regards,

Neo

 

0 项奖励
回复
1 解答
3,167 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

when the supply voltage is 3.3V, the MCU is not 5V tolerant even if a pin is configured as open drain. The datasheet explicitly states that open drain pin must be pulled to VDD. And Vih spec says that input voltage can't exceed VDD+0.3V. If an external circuit requires 5V, the only options are either to use 5V supply voltage for MCU or use some voltage level translator.

Regards,

Lukas

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,168 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

when the supply voltage is 3.3V, the MCU is not 5V tolerant even if a pin is configured as open drain. The datasheet explicitly states that open drain pin must be pulled to VDD. And Vih spec says that input voltage can't exceed VDD+0.3V. If an external circuit requires 5V, the only options are either to use 5V supply voltage for MCU or use some voltage level translator.

Regards,

Lukas

0 项奖励
回复
3,125 次查看
nanjun
Contributor III

Hello Lucas,

thanks for your reply. Actualley I wrote you back some days before but it seems the email failed.

The problem was solved.

Kind regards,

Neo

 

 

0 项奖励
回复