S32K144 and DFlash/PFlash prefetch buffer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K144 and DFlash/PFlash prefetch buffer

2,666件の閲覧回数
enricoantonioli
Contributor III

Hello,

when I write DFlash/PFash memory (with FCCOB registers) is it mandatory to disable the respective prefetch buffers?

Best regards,

E.

0 件の賞賛
返信
1 返信

2,334件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Enrico,

The Flash commands do not update the content of the buffers.
For example, with the buffers enabled, if a PFlash address is read, then reprogrammed and read again, both read accesses will return the same data.
Because the single-entry buffer can store the previously read data (Section 35.2.1 RM, rev.9).
So, this is on the user’s responsibility.

Regards,
Daniel

0 件の賞賛
返信