[S32K144] RTD missing LinIf.xdm, Tresos can't create module LinIf

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

[S32K144] RTD missing LinIf.xdm, Tresos can't create module LinIf

跳至解决方案
409 次查看
nbgddddd
Contributor I

Hello,

 

I have a question regarding the usage of LinIf plugin from the RTD in Tresos.

When trying to add LinIf module in Tresos it returns the following error:

nbgddddd_0-1743507161812.png

Module "LinIf_TS_T40D2M30I0R0" (defined in plugin "LinIf_TS_T40D2M30I0R0") defines the schema file "config/LinIf.xdm" which cannot be found (if the file is signed or crypted, it must be referenced in META-INF\CRYPTOMANIFEST.MF).

 

Unlike other modules, LinIf folder does not have a config folder where LinIf.xdm should have been

nbgddddd_1-1743507282665.png

Is ths a wrong installation or should the LinIf.xdm be generated separately somehow?

There is no LinIf.xdm in older RTD installations either.

 

Thanks!

 

 

0 项奖励
回复
1 解答
392 次查看
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @nbgddddd,

Please refer to the release notes for the RTD release (Version 3.0.0). You can see in the "Support and Delivered drivers" section, the LinIf driver delivered with the RTD is only a stub, it does not support configuration.

Julin_AragnM_0-1743528691712.png

This is only for testing purpose from our side. You should use CanIf, EthIf & LinIf from a third-party provider, such as Elektrobit (EB), Vector, etc. 

Best Regards,
Julián

在原帖中查看解决方案

1 回复
393 次查看
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @nbgddddd,

Please refer to the release notes for the RTD release (Version 3.0.0). You can see in the "Support and Delivered drivers" section, the LinIf driver delivered with the RTD is only a stub, it does not support configuration.

Julin_AragnM_0-1743528691712.png

This is only for testing purpose from our side. You should use CanIf, EthIf & LinIf from a third-party provider, such as Elektrobit (EB), Vector, etc. 

Best Regards,
Julián