S32K144: Question about DAC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K144: Question about DAC

ソリューションへジャンプ
4,159件の閲覧回数
sripav-7
Contributor III

Hello,

I understand that the DAC can be used to provide a reference voltage for use in the comparator. My question is, can I use the DAC to convert the digital data I have on my program into analog form and output it from a physical pin? If yes, please guide me.

Thank you,

Sri Harsha Pavuluri

ラベル(1)
タグ(1)
1 解決策
3,913件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,
The DAC is a sub-block of the comparator and its output is available as an internal signal only, it is not available externally on a pin.

Regards,
Daniel

元の投稿で解決策を見る

2 返答(返信)
3,914件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,
The DAC is a sub-block of the comparator and its output is available as an internal signal only, it is not available externally on a pin.

Regards,
Daniel

3,913件の閲覧回数
sripav-7
Contributor III

Guess I will have to use a PWM DAC then. Thank you!

0 件の賞賛
返信