S32K144 P_FLASH write data

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 P_FLASH write data

2,169 Views
玉敏111田
Contributor III

When I write to P_flash(Address 0x19000, 8 bytes),it can write successfullt.

But when the address is 0x190001, the byte can't be writen.

Why?

1 Reply

1,945 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi,

The address 0x190001 is out of Flash address range. I assume that you mean the address 0x19001.

Please, refer to the reference manual rev9. to the section "36.5.11.4 Program Phrase command" in that case.

There can be seen the note "1." under the "Table 36-40. Program Phrase Command FCCOB requirements"

The Flash address Must be 64-bit aligned (Flash address [2:0] = 000)

Also, if Flash address is not 64-bit aligned the FSTAT[ACCERR] bit is set.

Please, refer to "Table 36-41. Program Phrase command error handling".

I hope it helps you.

Best Regards,

Diana