S32K144 FlexIO instance limitation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K144 FlexIO instance limitation

ソリューションへジャンプ
2,560件の閲覧回数
Andy_Wang_JP
Contributor III

Hi 

I got a little question about S32K FlexIO module.

I've check the S32K RM,and it says FlexIO only have 1 instance.

But it that possible to implement 2 different module by using FlexIO?? 

For example: PTA 0/1/2/3 implement FlexIO SPI module and PTD1 implement FlexIO PWM.

Thanks and Waiting for reply

Andy

0 件の賞賛
返信
1 解決策
2,552件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Andy_Wang_JP

        Of course, there are already such routines in S32DS IDE. In this example, the FlexIO module is used to implement two-way I2S.

Senlent_1-1627959061038.png

 

 

 

 

 

 

 

 

    

BR!

    Jim.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,553件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Andy_Wang_JP

        Of course, there are already such routines in S32DS IDE. In this example, the FlexIO module is used to implement two-way I2S.

Senlent_1-1627959061038.png

 

 

 

 

 

 

 

 

    

BR!

    Jim.

0 件の賞賛
返信
2,536件の閲覧回数
Andy_Wang_JP
Contributor III

Hi @Senlent 

Thanks~

I've used that to implement my project

0 件の賞賛
返信