S32K144 FlexCAN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K144 FlexCAN

8,647件の閲覧回数
Alex19
Contributor II

Hello NXP,

I need your help, please. My problem is receiving several CAN messages PERIODICALLY without filtering.  It means, for example, i have 10 CAN messages with different period 50ms, 100ms, 500ms. If I take, for example, CAN ID = 0x101 and I receive with filtering, i receive periodically, but if I receive without filtering, this CAN message is received non periodically.  

0 件の賞賛
返信
15 返答(返信)

8,637件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Alex19

This can indeed happen if you don't set the mask for each MBs, which is not the correct way to set it.

In order to meet your design requirements, you can refer to this demo

https://community.nxp.com/t5/S32K-Knowledge-Base/S32K1xx-FlexCAN-Mask-Setting-Demo/ta-p/1519753 

Chapter:4.2.Set the Mask Type to Individual Mask Type.

0 件の賞賛
返信

8,638件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Alex19

This can indeed happen if you don't set the mask for each MBs, which is not the correct way to set it.

In order to meet your design requirements, you can refer to this demo

https://community.nxp.com/t5/S32K-Knowledge-Base/S32K1xx-FlexCAN-Mask-Setting-Demo/ta-p/1519753 

Chapter:4.2.Set the Mask Type to Individual Mask Type.

0 件の賞賛
返信

8,632件の閲覧回数
Alex19
Contributor II

Thank you for your response, 

I don't understand about 

4.1.Set the Mask Type to Global Mask Type.

     In this case, we can only receive the messages which ID from 0x300~0x37F and 0x400~0x47F.

but what if i want to receive for example 0x001~0x399 0x480~0x7FF. The idea is to identify the IDs and periods of the receiving CAN messages in a range  0x001~0x7FF. 

0 件の賞賛
返信

8,627件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

If you want to receive all IDs, you can set the mask to all 0

0 件の賞賛
返信

8,625件の閲覧回数
Alex19
Contributor II

like this?

 

FLEXCAN_DRV_Init(INST_CANCOM1, &canCom1_State, &canCom1_InitConfig0);

FLEXCAN_DRV_SetRxMaskType(INST_CANCOM1, FLEXCAN_RX_MASK_GLOBAL); 
FLEXCAN_DRV_SetRxMbGlobalMask(INST_CANCOM1, FLEXCAN_MSG_ID_STD, 0);

flexcan_data_info_t dataInfo =
{
.data_length = 8U,
.msg_id_type = FLEXCAN_MSG_ID_STD,
.enable_brs = false,
.fd_enable = false,
.fd_padding = 0U,
.is_remote = false
};

FLEXCAN_DRV_ConfigRxMb(INST_CANCOM1,RX_MAILBOX, &dataInfo, 0x7FF);

 

0 件の賞賛
返信

8,604件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Yes, all ID messages can be received in this way, but frame loss will occur if the speed is too fast, and this is not the correct way to use it. The recommended approach is to set one MB for each ID and set the mask value to all 1s.

0 件の賞賛
返信

8,597件の閲覧回数
Alex19
Contributor II

The idea is receive several CAN messages, and identify IDs of messages. If i want receive 40 messages, but there are just 32 MB, so I can't set one MB for each ID, with my understanding. 

0 件の賞賛
返信

8,563件の閲覧回数
Alex19
Contributor II

hello @Senlent ,

 

Can you clarify, please, about your last message

The recommended approach is to set one MB for each ID and set the mask value to all 1s. 

0 件の賞賛
返信

8,558件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

for example:

FLEXCAN_DRV_SetRxMaskType(INST_CANCOM1,FLEXCAN_RX_MASK_INDIVIDUAL);

FLEXCAN_DRV_ConfigRxMb(INST_CANCOM1, mb_idx_1, &dataInfo, msg_id_1);
FLEXCAN_DRV_SetRxIndividualMask(INST_CANCOM1,FLEXCAN_MSG_ID_STD,mb_idx_1,0xFFFFFFFF);

FLEXCAN_DRV_ConfigRxMb(INST_CANCOM1, mb_idx_1, &dataInfo, msg_id_2);
FLEXCAN_DRV_SetRxIndividualMask(INST_CANCOM1,FLEXCAN_MSG_ID_STD,mb_idx_2,0xFFFFFFFF);
...............
0 件の賞賛
返信

8,552件の閲覧回数
Alex19
Contributor II

Hello @Senlent 

Thank you very much for your answer.

FLEXCAN_DRV_SetRxMaskType(INST_CANCOM1,FLEXCAN_RX_MASK_INDIVIDUAL);

FLEXCAN_DRV_ConfigRxMb(INST_CANCOM1, mb_idx_1, &dataInfo, msg_id_1);
FLEXCAN_DRV_SetRxIndividualMask(INST_CANCOM1,FLEXCAN_MSG_ID_STD,mb_idx_1,0xFFFFFFFF);

FLEXCAN_DRV_ConfigRxMb(INST_CANCOM1, mb_idx_1, &dataInfo, msg_id_2);
FLEXCAN_DRV_SetRxIndividualMask(INST_CANCOM1,FLEXCAN_MSG_ID_STD,mb_idx_2,0xFFFFFFFF);

this configuration is for receiving CAN messages with filtering, but I need receiving without filtering. 

タグ(1)
0 件の賞賛
返信

8,546件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

We've discussed filtering and not filtering, I don't know that your problem is not solved yet.
You can send me your demo, I will reproduce this problem first, and I will think about whether there is any way to improve it.

0 件の賞賛
返信

8,539件の閲覧回数
Alex19
Contributor II

@Senlent 

I attached the poject 

 

0 件の賞賛
返信

8,524件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

I read your code, there are many problems, I can not help you to modify directly. I suggest you refer to the routine of interrupt sending and receiving, you can set the mask to all 0 (if you don't want to set the mask)

0 件の賞賛
返信

8,514件の閲覧回数
Alex19
Contributor II

Hello @Senlent ,

 

What do you mean use interrupt sending and receiving, it's use RxFIFO? 

0 件の賞賛
返信

8,506件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

You can use MB or FIFO to interrupt receiving and sending, I suggest you read the demo in my previous answer

0 件の賞賛
返信