S32K144 Flash Partitioning Example issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 Flash Partitioning Example issue

2,574 Views
Punit_01
Contributor II

While going through the example code for S32K Flash Partitioning in S32DS, I found an issue with the generated config file (peripherals_flash_FTFC.c).

The flash configuration is generated as below :

/* Flash user configuration 0 */
const flash_user_config_t Flash_InitConfig0 =
{
.PFlashBase = 0x0U,
.PFlashSize = 0x80000U,
.DFlashBase = 0x10000000U,
.EERAMBase = 0x14000000U,
.CallBack = NULL
};

Here, the CallBack is asigned a value equivalent to NULL => (((void *)0)

In the file flash_driver.c, to check if we have defined a callback or not, the comparision is done with 

NULL_CALLBACK.

if (NULL_CALLBACK != pSSDConfig->CallBack)
{
(pSSDConfig->CallBack)();
}

Upon executing this example from RAM, my code is going into a fault. When i made the necessary correction, it seems to work ok.

I believe it should either be NULL or NULL_CALLBACK but same should be used everywhere.

Is there something which I am missing or is there a genuine issue here?

Kindly help.

Tags (3)
0 Kudos
Reply
3 Replies

2,558 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

What version of S32K1 SDK are you using? Looks like it's fixed in newer versions of the SDK (I imported the flash_partitioning_s32k144 example with S32DS v3.4 + S32K1 SDK RTM 4.0.3)

FLASH SDK NULL callback.pngFLASH SDK NULL callback.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,553 Views
Punit_01
Contributor II

Hi Robin,

I am using below versions:

S32K144_SDK v4.0.1 with S32Ds v3.5.

Thanks for your quick support.

0 Kudos
Reply

2,550 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Currently S32DS v3.5 cannot update S32K1 SDK to the latest RTM 4.0.3 version, so I suggest you use S32DS v3.4.
Sorry for the inconvenience we bring you!

0 Kudos
Reply