S32K144 EVB - CAN example code with MC33903 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 EVB - CAN example code with MC33903 ?

2,885 Views
sukkinpang
Contributor I

I've just received the S32K144 EVB and downloaded the S32 Design Studio 1.3.

In the example code it initialise the MC33903 but I can't find a MC33903 on the dev board, only a UJA1169.

Is there any example code to initialise the UJA1169?

Sukkin

Tags (2)
0 Kudos
Reply
1 Reply

1,923 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

there are some projects in SDK examples:

c:\NXP\S32DS_ARM_v1.3\S32DS\S32_SDK_Beta_0.9.0\examples\S32K144\demo_apps\FlexCan\

Release of SDK EAR 0.8.2 is compatible with UJA1169 and MC33903/4/5.

There was MC33903 on first version of EVB (S32K144 rev1 was used). Next version of board (with S32K144 rev2) uses UJA1169 to improve CAN-FD capabilities - this is the one you have.

In next release BETA 0.9.0 the support of MC33903/4/5 is removed.

Regards,

Lukas

0 Kudos
Reply