S32K144: Cannot access device after mass erase(CSEc enabled, with no master key loaded)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K144: Cannot access device after mass erase(CSEc enabled, with no master key loaded)

跳至解决方案
2,417 次查看
nschwabe
Contributor I

Hello,

I have an S32K144 device where the program partition command (PGMPART) was used to allocate CSEc with keysize = 1 to 20.

But no MASTER_ECU_KEY was installed. That means no CMD_LOAD_KEY was executed.

Afterwards a mass erase was issued using a JLink debugger and the `Erase` command

Now the debugger cannot connect and displays the following:

$ JLinkExe -if swd -device "S32K144 (allow security)" -speed 4000 -autoconnect 1
破坏者
SEGGER J-Link Commander V7.80d (Compiled Oct 4 2022 16:40:45)
DLL version V7.80d, compiled Oct 4 2022 16:40:22

Connecting to J-Link via USB...O.K.
Firmware: J-Link V10 compiled Sep 22 2022 14:59:36
Hardware version: V10.10
J-Link uptime (since boot): N/A (Not supported by this model)
S/N: 50124738
License(s): GDB
VTref=4.982V
Device "S32K144 (ALLOW SECURITY)" selected.


Connecting to target via SWD
InitTarget() start
Device will be unsecured now.
InitTarget() end
Found SW-DP with ID 0x2BA01477
DPIDR: 0x2BA01477
CoreSight SoC-400 or earlier
Scanning AP map to find all available APs
AP[2]: Stopped AP scan as end of AP map has been reached
AP[0]: AHB-AP (IDR: 0x24770011)
AP[1]: JTAG-AP (IDR: 0x001C0000)
Iterating through AP map to find AHB-AP to use
AP[0]: Skipped. Could not read CPUID register
AP[1]: Skipped. Not an AHB-AP
InitTarget() start
Device will be unsecured now.
Timeout while halting CPU.
InitTarget() end
Found SW-DP with ID 0x2BA01477
DPIDR: 0x2BA01477
CoreSight SoC-400 or earlier
Scanning AP map to find all available APs
AP[2]: Stopped AP scan as end of AP map has been reached
AP[0]: AHB-AP (IDR: 0x24770011)
AP[1]: JTAG-AP (IDR: 0x001C0000)
Iterating through AP map to find AHB-AP to use
AP[0]: Skipped. Could not read CPUID register
AP[1]: Skipped. Not an AHB-AP

****** Error: Could not find core in Coresight setup

InitTarget() start
Device will be unsecured now.
Timeout while halting CPU.
InitTarget() end
Found SW-DP with ID 0x2BA01477
DPIDR: 0x2BA01477
CoreSight SoC-400 or earlier
Scanning AP map to find all available APs
AP[2]: Stopped AP scan as end of AP map has been reached
AP[0]: AHB-AP (IDR: 0x24770011)
AP[1]: JTAG-AP (IDR: 0x001C0000)
Iterating through AP map to find AHB-AP to use
AP[0]: Skipped. Could not read CPUID register
AP[1]: Skipped. Not an AHB-AP
InitTarget() start
Device will be unsecured now.
Timeout while halting CPU.
InitTarget() end
Found SW-DP with ID 0x2BA01477
DPIDR: 0x2BA01477
CoreSight SoC-400 or earlier
Scanning AP map to find all available APs
AP[2]: Stopped AP scan as end of AP map has been reached
AP[0]: AHB-AP (IDR: 0x24770011)
AP[1]: JTAG-AP (IDR: 0x001C0000)
Iterating through AP map to find AHB-AP to use
AP[0]: Skipped. Could not read CPUID register
AP[1]: Skipped. Not an AHB-AP

****** Error: Could not find core in Coresight setup

Cannot connect to target.

 Is it possible to recover this device?

 

As pointed out in this answer it is not possible to reset the partition without the master key. But I think this scenario is a little different because of the mass erase.

0 项奖励
回复
1 解答
2,401 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @nschwabe 

Once CSEc is enabled by PGMPART command, the mass erase is blocked until the partition is destroyed by CMD_DBG_CHAL and CMD_DBG_AUTH commands with knowledge of MASTER_ECU_KEY. So, JLink definitely could not perform mass erase. If the flash was erased by Erase Flash Block or by Erase Flash Sector commands leaving the Flash Configuration Field at 0x400 erased, the device is secured (because FSEC byte in the Flash Configuration Field is 0xFF and not in unsecured state 0xFE) while mass erase command is disabled due to CSEc. The result: the device is bricked with no way to recover.

Regards,

Lukas

在原帖中查看解决方案

3 回复数
2,402 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @nschwabe 

Once CSEc is enabled by PGMPART command, the mass erase is blocked until the partition is destroyed by CMD_DBG_CHAL and CMD_DBG_AUTH commands with knowledge of MASTER_ECU_KEY. So, JLink definitely could not perform mass erase. If the flash was erased by Erase Flash Block or by Erase Flash Sector commands leaving the Flash Configuration Field at 0x400 erased, the device is secured (because FSEC byte in the Flash Configuration Field is 0xFF and not in unsecured state 0xFE) while mass erase command is disabled due to CSEc. The result: the device is bricked with no way to recover.

Regards,

Lukas

2,237 次查看
ZEROOO
Contributor IV

Hi lukaszadrapa

    If the CSEc partition command is executed, and the master key command is not executed, after brushing into the MCU, if I want to erase the partition, is it valid to reprogram and set the master key to load and then execute the erase command?

0 项奖励
回复
2,364 次查看
nschwabe
Contributor I

Hi @lukaszadrapa,

thanks for the explanation.

This matches pretty much what I observed. I used the JLink Erase command which probably erases individual sectors leaving the device in secured state.

When I connect the JLink, I get a message that I need to mass erase the device. And I know understand that this operation is blocked by the CSEc partitioning.

Thanks again!

0 项奖励
回复