S32K144 CAN MASTER Sample Code

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K144 CAN MASTER Sample Code

5,416 次查看
yash_bhatnagar9
Contributor II

Hi, Can anyone provide the link to the CAN Master and CAN Slave Sample code examples. I am unable to find the links to them.

标记 (2)
0 项奖励
回复
5 回复数

4,866 次查看
ArSa
Contributor II

Hello Robin, 

Thanks for the response. From the links you have helped with it seems easy to start with an Example code. But I am having multiple issues after updating my S32DS to 3.5.

 

Firstly when I Help -> check for updates will lead to following error log.

Some sites could not be found. See the error log for more detail.
No repository found at http://www.nxp.com/lgfiles/updates/Eclipse/APSW/S32DS_3.5.
HTTP Server 'Bad Gateway' : http://gnuarmeclipse.sourceforge.net/updates/content.xml
HttpComponents connection error response code 502.

 

and Secondly when I look for Example projects the following is the view,

FrustatedEngineer_0-1665922790536.png

 

It seems something is missing in whole. Please help me in fixing the issue

 

0 项奖励
回复

4,859 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Please ask on the S32 Design Studio forum about this issue.

0 项奖励
回复

4,897 次查看
ArSa
Contributor II

I have the error Cpu.h is not found, neither i could find it in whole C:/NXP folder. where can i find it

0 项奖励
回复

4,888 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport
0 项奖励
回复

5,407 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi yash_bhatnagar9,

Please refer the can_pal_s32k144 example of S32SDK. 
You can download the S32 Design Studio 3.4 and then install the S32SDK S32K1XX RTM 4.0.1 in S32DS Extensions and Updates view.

can_pal_s32k144.pngdefine MASTER SLAVE.pngS32DS Extensions and Updates.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复