S32K144 CAN FD issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 CAN FD issue

5,196 Views
liulei1
Contributor II

Hello
I would like to receive CAN FD Standard ID using Filter.

 

An ID (0x100 ~ 0x6FF) exists in the bus
I try to receive each filter using different filters from 0x100 to 0x1FF, 0x200 to 0x2FF, 0x300 to 0x3FF, 0x400 to 0x4FF, 0x500 to 0x5FF, and 0x600 to 0x6FF for each filter.

Below is my code:

{
#define MBR0_BASE ((unsigned char *)0x40024080)

#define PL_LEN_8 16
#define PL_LEN_16 24
#define PL_LEN_32 40
#define PL_LEN_64 72

#define CAN0_MBR0(pl, idx) ((MB_Struct*)((MBR0_BASE) + (PL_LEN_##pl) * (idx)))
unsigned long i;

/* Activate Clock for FlexCAN and PORT */
PCC->PCCn[PCC_FlexCAN0_INDEX] |= PCC_PCCn_CGC_MASK;
if(portn == PTE4_PTE5_CAN)
{
PCC->PCCn[PCC_PORTE_INDEX] |= PCC_PCCn_CGC_MASK;
PORTE->PCR[4] |= PORT_PCR_MUX(5);
PORTE->PCR[5] |= PORT_PCR_MUX(5);
}
else if(portn == PTC2_PTC3_CAN)
{
PCC->PCCn[PCC_PORTC_INDEX] |= PCC_PCCn_CGC_MASK;
PORTC->PCR[2] |= PORT_PCR_MUX(3);
PORTC->PCR[3] |= PORT_PCR_MUX(3);
}

CAN0->MCR |= CAN_MCR_MDIS_MASK; /* MDIS=1: Disable module before selecting clock */

CAN0->CTRL1 |= CAN_CTRL1_CLKSRC_MASK; /* CLKSRC=1: Clock Source = BUSCLK (40 MHz) */

CAN0->MCR &= ~CAN_MCR_MDIS_MASK; /* MDIS=0; Enable module config. (Sets FRZ, HALT)*/

while (!((CAN0->MCR & CAN_MCR_FRZACK_MASK) >> CAN_MCR_FRZACK_SHIFT)) {}

/* Good practice: wait for FRZACK=1 on freeze mode entry/exit */

CAN0->CBT = 0x802FB9EF; /* Configure nominal phase: 500 KHz bit time, 40 MHz Sclock */

/* Prescaler = CANCLK / Sclock = 80 MHz / 40 MHz = 2 */

/* EPRESDIV = Prescaler - 1 = 2 - 1 = 1 */

/* EPSEG2 = 15 */

/* EPSEG1 = 15 */

/* EPROPSEG = 46 */

/* ERJW = 15 */

/* EPRESDIV= 3 CAN0->CBT= 0x80685CE7 koor*/

/* BITRATEn =Fcanclk /( [(1 + (EPSEG1+1) + (EPSEG2+1) + (EPROPSEG + 1)] x (EPRESDIV+1)) */

/* = 80 MHz /( [(1 + ( 15 +1) + ( 15 +1) + ( 46 + 1)] x ( 1 +1)) */

/* = 80 MHz /( [1+16+16+47] x 2) = 80 MHz /(80x2) = 500 Kz */

CAN0->FDCBT = 0x00131CE3; /* Configure data phase: 2 MHz bit time, 40 MHz Sclock */

/* Prescaler = CANCLK / Sclock = 80 MHz / 40 MHz = 2 */

/* FPRESDIV = Prescaler - 1 = = 2 - 1 = 1 */

/* FPSEG2 = 3 */

/* FPSEG1 = 7 */

/* FPROPSEG = 7 */

/* FRJW = 3 */

/* BITRATEf =Fcanclk /( [(1 + (FPSEG1+1) + (FPSEG2+1) + (FPROPSEG)] x (FPRESDIV+!)) */

/* = 80 MHz /( [(1 + ( 7 +1) + ( 3 +1) + ( 7 )] x ( 1 +1)) */

/* = 80 MHz /( [1+8+4+7] x 2) = 80 MHz /(20x2) = 80 MHz / 40 = 2 MHz */

CAN0->FDCTRL =0x80030500; /* Configure bit rate switch, data size, transcv'r delay */

/* BRS=1: enable Bit Rate Swtich in frame's header */

/* MBDSR1: Not applicable */

/* MBDSR0=3: Region 0 has 64 bytes data in frame's payload */

/* TDCEN=0: disable Transceiver Delay Compensation */

/* TDCOFF=5: 5 CAN clocks (300us) offset used */


for (i=0; i<7; i++)
{
CAN0_MBR0(64, i)->CS.R = 0;
CAN0_MBR0(64, i)->ID.R = 0;
}
for(i=0; i<16; i++ ) /* Initialize all of 16 Individual Filter Mask */
{
CAN0->RXIMR[i] = 0x1FFFFFFF; /* Disable Filter Mask */
}

CAN0_MBR0(64, 2)->CS.B.EDL = 1; /* 1: CAN FD frame */
CAN0_MBR0(64, 2)->CS.B.BRS = 1; /* 1: CAN FD frame Bode Rate Switch Enable */
CAN0_MBR0(64, 2)->CS.B.IDE = 0; /* Use standard ID length */
CAN0_MBR0(64, 2)->ID.B.ID_STD = 0x10; /* receive ID is 0x123 */
CAN0_MBR0(64, 2)->CS.B.CODE = 0x4;

CAN0->RXMGMASK = 0x1FFFFFFF;//0x1FFFFFFF; /* Global acceptance mask */
CAN0->IMASK1 = 0x0000000E; /* MB 3 for CAN0 interrupt Enable */

CAN0->CTRL2 |=CAN_CTRL2_ISOCANFDEN_MASK; /* Enable CRC fix for ISO CAN FD */

CAN0->MCR = 0x0002081F;//0x0002081F; /* Negate FlexCAN 1 halt state & enable CAN FD for 32 MBs */

while ((CAN0->MCR & CAN_MCR_FRZACK_MASK) >> CAN_MCR_FRZACK_SHIFT) {}

/* Good practice: wait for FRZACK to clear (not in freeze mode) */

while ((CAN0->MCR & CAN_MCR_NOTRDY_MASK) >> CAN_MCR_NOTRDY_SHIFT) {}


INT_SYS_EnableIRQ(CAN0_ORed_0_15_MB_IRQn);
}

Labels (1)
0 Kudos
Reply
2 Replies

4,801 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

what is the issue? Do you see any kind of error?

Are you able to receive standard ID=0x10 message you defined?

Did you check that correct MB address is written and both CS and ID words have correct values?

For the filtering scheme...

You do not set MCR[IRMQ] so individual mask registers are not used and masking is based on RXMGMASK, RX14MASK and RX15MASK.

To achieve filter ranges from 0x100 to 0x1FF, 0x200 to 0x2FF, 0x300 to 0x3FF, 0x400 to 0x4FF, 0x500 to 0x5FF, and 0x600 to 0x6FF you need to set 6 MBs and use corresponding 6 RXIMRs. Global mask can be used to as it will be the same. Setting will be

MB0.CS.B.IDE=0

MB0.ID.R = 0x100 << 18;

RXIMR0 = 0 | (0x700<<18);   // lower 8 bits of standard ID is don't care

MB1.CS.B.IDE=0

MB1.ID.R = 0x200 << 18;

RXIMR1 = 0 | (0x700<<18);

similarly for other MBs to cover other ID ranges

BR, Petr

0 Kudos
Reply

4,371 Views
miaoming
Contributor I

Hello,

    Could you please tellme where to get the definication of MB_Struct ?

Thank you

 

==============================

 And AN5413 has something wrong in 

 

#ifdef NODE_A /* Node A receives msg with std ID 0x511 */
CAN0->RAMn[ 4*MSG_BUF_SIZE + 1] = 0x14440000; /* Msg Buf 4, word 1: Standard ID = 0x111 */  <-- should be 0x511
 
 
Tags (1)
0 Kudos
Reply