S32K144 Bus fault during instruction prefetch while using LPIT0 ISR.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 Bus fault during instruction prefetch while using LPIT0 ISR.

4,176 Views
lucianomoretti
Contributor IV

I'm having an issue where I'm getting a bus fault after enabling the LPIT0 ISR. The timing of the issue is not consistent: sometimes I'll run for a second or two, sometimes I'll run for 10+ seconds. Using a modified version of the AN12218 Bootloader.

Debugger shows my LPIT0_Ch0_IRQHandler called, then another signal handler called for the default handler (I'm guessing it's the Hard Fault Handler)

S32 Design Studio for ARM reports the following on the console:
BusFault: A bus fault has occurred during instruction prefetching.

CFSR is 0x00000100

HFSR is 0x40000000

I'm enabling it using the following code similar to the code used in the AN5413 S32K1xx Series Cookbook section 2.3:

	/* set up interrupt handling for the timer */

	S32_NVIC->ICPR[1] = 1 << (48 % 32); /* IRQ48-LPIT0 ch0: clr any pending IRQ*/
	S32_NVIC->ISER[1] = 1 << (48 % 32); /* IRQ48-LPIT0 ch0: enable IRQ */
	S32_NVIC->IP[48] =0x0A; /* IRQ48-LPIT0 ch0: priority 10 of 0-15*/

	/* Enable bus clock to PIT */
	PCC->PCCn[PCC_LPIT_INDEX] = PCC_PCCn_PCS(3) | PCC_PCCn_CGC_MASK;    /* Clock src=3 (FIRC_DIV2_CLK)*/

	/* Turn on PIT */
	LPIT0->MCR |= LPIT_MCR_M_CEN_MASK; /* enable module clock */
	LPIT0->MIER = 0x00000001; /* TIE0=1: Timer Interrupt Enabled for Chan 0 */

	/* Configure Channel 0 to trigger as defined in pit.h */
	LPIT0->TMR[0].TVAL = TRIG_PERIOD;

	/* Enable timer */
	LPIT0->TMR[0].TCTRL = LPIT_TMR_TCTRL_T_EN_MASK;

ISR Code is:

void LPIT0_Ch0_IRQHandler (void) {
	if(LPIT0->MSR & LPIT_MSR_TIF0_MASK){
		LPIT0->MSR |= LPIT_MSR_TIF0_MASK; /* Clear LPIT0 timer flag 0 */
		is_triggered = 1;
	}
}

is_triggered is a volatile int that's only accessed from one function in the regular code which is not in the call chain when the fault occurs (access has a disable interrupts and put a dsb & isb after disabling interrupts)

When it happens I'm performing a Flash Command Sequence in fsl_flash_driver_c90tfs.c (Copyright 2016), but that's the main thing that the bootloader is doing.

0 Kudos
Reply
2 Replies

4,162 Views
lucianomoretti
Contributor IV

Thanks for the info.

I managed to get the behavior I wanted using the polling solution so when I have time I'll go back and try to figure out what was going on. I'm not masking any interrupts during the flash process.

I got the S32_NVIC->IP settings directly from AN5413 S32K1xx Series Cookbook, Rev. 5. Probably should add that to the list of things to fix/revise.

0 Kudos
Reply

4,168 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @lucianomoretti,

Are the interrupts masked while the flash is being programmed?

 

You can analyze the fault exception further following this example:

https://community.nxp.com/t5/S32K-Knowledge-Base/Fault-handling-on-S32K14x/ta-p/1114447

Since it is a precise bus fault, the S32_SCB_BFAR register holds an address of the fault memory access.

And you should be able get the fault instruction too.

 

By the way, the priority of the LPIT interrupt is not set correctly.

The priority number must be in the 4 MSBs of the IP register.

S32_NVIC->IP[48] = 0xA0; /* IRQ48-LPIT0 ch0: priority 10 of 0-15*/

 

Regards,

Daniel

0 Kudos
Reply