S32K144 AMMCLIB MLIB_Div_F32() Precision Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 AMMCLIB MLIB_Div_F32() Precision Problem

2,837 Views
420113461
Contributor I

When using ammclib tool library for division calculation, the last 15 bit(bit14 --- bit0) results of each calculation are 0, and the actual accuracy is only 16 bit(bit30 --- bit15).

code.pngcode.pngdebug.pngdebug.png

0 Kudos
Reply
4 Replies

2,635 Views
petrz_
NXP Employee
NXP Employee

Hi,

we added a new library function MLIB_DivSatAccurate_F32 in the AMMCLib release 1.1.26. This function calculates the division with full 32-bit accuracy of the result. The function is faster than 64-bit by 32-bit division (if you relied on compiler's optimization capabilities) but not as fast as MLIB_DivSat_F32.

0 Kudos
Reply

2,832 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I can see it corresponds to the description. There's a note:

lukaszadrapa_0-1599544210237.pnglukaszadrapa_0-1599544210237.png

 

Regards,

Lukas

 

0 Kudos
Reply

2,826 Views
420113461
Contributor I

What's the difference between the three versions of ammclib library? Will it improve the calculation accuracy?AMMCLIB.pngAMMCLIB.png

0 Kudos
Reply

2,818 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

There's no difference. It just means if you have want to get object code for evaluation or if you want to buy a license for production (either object code only or full source code).

Regards,

Lukas

 

0 Kudos
Reply