I'm trying to read analog pins PTD2(ADC1 channel2) and PTE6(ADC1 channel 11) using LPTMR, PDB1 and DMA . I'm using DMA loop transfer to move contents of ADC1->R[0] to an user created buffer. But I'm not getting DMA callback, which is supposed to be received after successful DMA transfer.
Can someone tell me, where I'm going wrong. I have attached the project code zip file below.