S32K142 FlexIO SPI driver initialization ERROR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K142 FlexIO SPI driver initialization ERROR

Jump to solution
3,788 Views
AndyChen1
Contributor I

Hello everyone:

Recently I am researching on S32K142 flexio SPI configuration, master mode. 

Following configuration of  demo example, FLEXIO_SPI_DRV_MasterInit is always return ERROR. Does anyone knoes why and how could I solve it?

Details as follows:

1. Background

mcu: S32K142_64

IDE: S32 Design Studio V2.2

SDK version: RTM 3.0.0

2. Configuration

2.1 PinSettings:

AndyChen1_0-1700636919190.png

 

2.2 FlexIO spi configuration

AndyChen1_1-1700636967360.png

 

3. Code implementaion:

flexio_device_state_t flexIODeviceState;
flexio_spi_master_state_t flexIOSPIState_Master;

FLEXIO_DRV_InitDevice(INST_FLEXIO_SPI1, &flexIODeviceState);
FLEXIO_SPI_DRV_MasterInit(INST_FLEXIO_SPI1, &flexio_spi1_MasterConfig0, &flexIOSPIState_Master);

4. Question:

4.1

when I debug to FLEXIO_SPI_DRV_MasterInit-->FLEXIO_DRV_InitDriver-->FLEXIO_DRV_Allocate

FLEXIO_DRV_Allocate is always return ERROR. Regiater PARAM is all zero, It seems no shifter and timer resource is available for my configuration.

Any one knows why?

4.2

And when  I try to use FLEXIO_SPI_DRV_MasterTransferBlocking to send some dummy spi data, master->driverIdle is always TRUE, NO any signal according to scope. I dont know if it is related with 4.1 question?

 

Anyone help me? thanks a lot!

 

0 Kudos
Reply
1 Solution
3,736 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

It looks like you have old version of the chip. The 'R' in the part number means (FS32K142URT0VLH LQFP64) that it's device with "Basic feature set" only without FlexIO. This version is not offered anymore:

lukaszadrapa_0-1700821312417.png

 

So, my recommendation is to order new device. As you can see in the screenshot above, all current devices have FlexIO available now (see Y: Optional feature).

Regards,

Lukas

View solution in original post

0 Kudos
Reply
5 Replies
3,787 Views
AndyChen1
Contributor I

Update on 4.2

 

master->driverIdle is always FALSE in function FLEXIO_SPI_DRV_MasterTransferBlocking

-------------------------------------------------------- update above------------------------------------------------------

4.2

And when  I try to use FLEXIO_SPI_DRV_MasterTransferBlocking to send some dummy spi data, master->driverIdle is always TRUE, NO any signal according to scope. I dont know if it is related with 4.1 question?

 

Tags (1)
0 Kudos
Reply
3,749 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @AndyChen1 

the most interesting information is that PARAM is always zero. Could you write down whole part number of your device?

Thanks,

Lukas

0 Kudos
Reply
3,744 Views
AndyChen1
Contributor I

Hello @lukaszadrapa 

whole part number is FS32K142URT0VLH LQFP64

 

I saw PARAM reset value is 0x04080404,

when I double click register name, the value read back is 0x0000000.

Is there any operation mistake or something I mis-understand?

AndyChen1_1-1700817754070.png

 

 

0 Kudos
Reply
3,737 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

It looks like you have old version of the chip. The 'R' in the part number means (FS32K142URT0VLH LQFP64) that it's device with "Basic feature set" only without FlexIO. This version is not offered anymore:

lukaszadrapa_0-1700821312417.png

 

So, my recommendation is to order new device. As you can see in the screenshot above, all current devices have FlexIO available now (see Y: Optional feature).

Regards,

Lukas

0 Kudos
Reply
3,698 Views
AndyChen1
Contributor I

Hello @lukaszadrapa 

Thanks for your kindly reply!

0 Kudos
Reply