S32K118 Micro Flashing Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K118 Micro Flashing Issue

1,987 Views
gadilinga
Contributor III

gadilinga_0-1722505152854.png

while flashing time I'm getting this type of error u can see the Above the pic plz guide me for Rectify. one time it is working second time flashing means it's not working. that is solution for this

0 Kudos
Reply
5 Replies

1,964 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

 

Hi

Note that these debug pins should be added to UnTouchedPortPin. Otherwise, you will not be able to connect to the S32K because the debug pins have changed to other functions after the pin initialization is done at power-up.

UnTouchedPortPin Debug pins.png

If so, please try to use the Kinetis_Recovery_Utility.zip mentioned in Can't use PEmicro debugger with S32K118EVB2-Q048

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,934 Views
gadilinga
Contributor III
Hi Robin,
thank u for u r reply but without adding the UnTouchedPortPin also previously its working. now its not working currently I'm using S32k118 Board. even though example also we flashed but also same issue.
0 Kudos
Reply

1,928 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

You may be experiencing the situation described in this post: Recovering Cortex-M Microcontroller with a Power Glitch:

Even worse: you can disable or re-mux the debug pins (maybe because you did not know what you are doing, or you wanted preventing unauthorized access, or you just needed these pins for something).

 Have you try to use P&E Recovery Utility halt MCU?

0 Kudos
Reply

1,905 Views
gadilinga
Contributor III

Hi @Robin_Shen ,

thank u for  fastest reply and Support to wards the solution. currently I'm not using debugger, so I configured Untouched pin still I'm facing same issue. once  its flashing when it suspend or terminated. second time again we need to plugs out and reconnect means it will work later. every time  we need to do like this.

0 Kudos
Reply

1,860 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

How about reset the MCU, for example press SW5?

0 Kudos
Reply