S32K118 - JTAG lock

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K118 - JTAG lock

跳至解决方案
6,675 次查看
JiriTak
Contributor II

Hello, is there chance to read out memory content if MCU is secured for JTAG connection using flash configuration bytes. Also is configured backdoor access key (which is known) and mass erase is disabled.

I am able to unlock MCU in application (content of FSEC_SEC is 10b) and also can perform mass erase from application. But I would like to have an option to connect to this device and read content of MCU using debugger. I am using the Segger j-link Plus debugger and IAR studio. Is it possible to be able e.g. via j-link commander to connect to MCU and read the memory content?

 

Thanks and regards,

Jiri

0 项奖励
回复
1 解答
6,643 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Once the MCU has been unlocked via the Backdoor key, it stays unlocked until the MCU is reset.

So, the debugger must not reset the MCU, the debugger has to be just attached to the running MCU.

Please read this article:

Attaching to a Running Target with Segger J-Link, GDB and Eclipse

https://mcuoneclipse.com/2015/03/20/attaching-to-a-running-target-with-segger-j-link-gdb-and-eclipse...

 

Thanks,

Daniel

在原帖中查看解决方案

0 项奖励
回复
6 回复数
6,641 次查看
JiriTak
Contributor II

Thank you for this, I will ask then Segger, if they can help me. I am using IAR Embeded Workbench and not Eclipse.

0 项奖励
回复
6,659 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Jiri,

The debugger cannot read the content of the MCU if the MCU is secure (FSEC_SEC != 10b).

The MCU needs to be unlocked first (FSEC_SEC == 10b).

The debugger can only mass erase the MCU to unlock it provided this option is enabled (FSEC_MEEN != 10b).

 

Regards,

Daniel

 

0 项奖励
回复
6,658 次查看
JiriTak
Contributor II

Hello Daniel,

yes I know about this. My question is, if debugger, can unlock device via JTAG/SWD?

Jiri

0 项奖励
回复
6,653 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Only through mass erase.

The debugger can access the MDM-AP status and control registers.

Please refer to the RM, Section 58.6.

 

Regards,

Daniel

0 项奖励
回复
6,648 次查看
JiriTak
Contributor II

Ok, another question. If I unlock MCU in application (e.g. sent via LIN/UART/... key, and sucessfully compared), will be able to read out memory? Tried using J-Flash, but it always return error, that it cannot access the memory.

0 项奖励
回复
6,644 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Once the MCU has been unlocked via the Backdoor key, it stays unlocked until the MCU is reset.

So, the debugger must not reset the MCU, the debugger has to be just attached to the running MCU.

Please read this article:

Attaching to a Running Target with Segger J-Link, GDB and Eclipse

https://mcuoneclipse.com/2015/03/20/attaching-to-a-running-target-with-segger-j-link-gdb-and-eclipse...

 

Thanks,

Daniel

0 项奖励
回复