S32K116EVB-Q048 can't connect to FreeMaster

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K116EVB-Q048 can't connect to FreeMaster

4,216 Views
brns
Contributor II

Hi

I am currently getting started with the S32K116EVB-Q048 (old version). However, when I try to establish connection to the board in FreeMaster, I always get the error ""No board detected on any of the specified UART communication ports".

I have alredy looked into this discussion S32K116EVB FreeMaster Connection Failure, however I couldn't solve the problem.

Additionally, where can I get the original code from NXP? The board was already used before me.

Thank you.

Tags (2)
0 Kudos
Reply
5 Replies

4,192 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please download the S32K116EVB Evaluation Board – Software for FreeMASTER(S32K116EVB_JumpStart_FreeMaster.zip).

Also take a look at the Q&A of S32K1x FreeMASTER JumpStart Project


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

4,173 Views
brns
Contributor II

Thank you for your response.

I had already downloaded  S32K116EVB Evaluation Board – Software for FreeMASTER and I did it again but I still can't connect the board.

Attached is the error I get in the Communication Debug Log and Connection Wizard.

I do have installed the most recent version of SD32 Design Studio, I don't know if that can influence the connection in FreeMaster.

Thank you.

 

0 Kudos
Reply

4,168 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Did you drop the S32K116_EVB_JumpStart_Firmware.srec(...\S32K116EVB_JumpStart_FreeMaster \S32K116_EVB_JumpStart_Firmware\Debug) into mass storage device?

S32K116_EVB_JumpStart_Firmware.srec S32K116EVB.png

After this, the RGB LED will blink.

0 Kudos
Reply

4,161 Views
brns
Contributor II

My company computer does not allow me to have full access to the ports, so I can't do that. Isn't there an alternative solution?

Thanks.

0 Kudos
Reply

4,147 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Install S32 Design Studio for Arm 2018.R1 – Windows/Linux and S32 Design Studio for ARM 2018.R1 - Update 11 by refer to Q&A of S32K1x FreeMASTER JumpStart Project

Debug ...\S32K116EVB_JumpStart_FreeMaster\S32K116_EVB_JumpStart_Firmware project.

0 Kudos
Reply