S32K116 mini system hardware design

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K116 mini system hardware design

866 次查看
Thalassa
Contributor I

Hi, I am new to S32K family. If I want to design a minimum hardware board for S32K116, is there an example circuit design to look at? Can I omit the external crystal? Which are the necessary external components needed for such mini system? I only need CAN and UART controller working.

thanks.

0 项奖励
回复
1 回复

856 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Thalassa,

You can refer: UCANS32K146 development system – Schematics (REV 1 ) 

For UART part, you can refer:S32K116EVB Evaluation Board – Schematics (REV 0 ) 

 

Can I omit the external crystal?
Not recommend. "The oscillator clock should be selected whenever a tight tolerance (up to 0.1%) is required in the CAN bus timing. The crystal oscillator clock has better jitter performance than the peripheral clock."

crystal oscillator clock.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复