Dear all:
My board can't boot up when power on,the appearence is showed below:
Here is the development enviroment:
Does anyone have the same problem? Or can you give me some ideas to solve it.
Best regard!
已解决! 转到解答。
Hi cheney,
Please check if caused by this:S32K118 runs with debugger, but not without
Please also check the debug interface and Reset_b\NMI_b part of circuit by refer to AN5426: Hardware Design Guidelines for S32K1xx – Application Note
Best Regards,
Robin
Hi cheney,
Please check if caused by this:S32K118 runs with debugger, but not without
Please also check the debug interface and Reset_b\NMI_b part of circuit by refer to AN5426: Hardware Design Guidelines for S32K1xx – Application Note
Best Regards,
Robin
Hi, Robin:
I add the macro "START_FROM_FLASH" in the assember, it works fine now. Thanks a lot.
Is it a bug in the IDE? I can see the macro defined in the C compiler preprocesser option, but the macro is only used in startup_S32K116.s and the macro is not defined in the assember Symbols.
Best Regards!
Cheney