S32K116 Reset issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K116 Reset issue

Jump to solution
9,211 Views
asd046012
Contributor III

Hello

    I meet a issue: the reset signal could not reset MCU.

    when I measued the pin reset, find that The voltage of the reset signal is 1V and the time is 500us,and the supply voltage of MCU is 5V.

    But I see the datasheet the range of low voltage  is 0-0.3VDD,so the I and hardware engineer all think the hardware design meet with the datasheet.

    so what is the requirement of the reset signal of MCU s32k116? could you tell me the corrent answer? 

 

 

0 Kudos
Reply
1 Solution
9,101 Views
asd046012
Contributor III

This issue has been solved, the pull-up resistance 22K has been replaced to resistance 22 by supplier, cause the level to not be low.

 I have used the resistance 22K to replace the resistance 22,the reset signal is normal.

 

View solution in original post

0 Kudos
Reply
7 Replies
9,102 Views
asd046012
Contributor III

This issue has been solved, the pull-up resistance 22K has been replaced to resistance 22 by supplier, cause the level to not be low.

 I have used the resistance 22K to replace the resistance 22,the reset signal is normal.

 

0 Kudos
Reply
9,198 Views
asd046012
Contributor III

Hello  Robin_Shen

    I see this file,  our system use 24MHz bus clock,  so I think 500us absolutely fit with time requirement of signal reset,  the low voltage is 0-0.3VDD(0-1.5v),the voltage also fit with the datasheet. Reset circuit is as below, signal reset_sbc is the input signal reset.

 

    So could you give me any advice?

  

 

Reset circuitReset circuit

 
 

 

 

 

 

0 Kudos
Reply
9,164 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

I am a little confused what is the role of BAT54W here. Will it works if you remove D0102?
As I know the reset_sbc and RESET_MC1(PTA5) are bidirectional.

0 Kudos
Reply
9,146 Views
asd046012
Contributor III

Hello

   Sorry for the delay response. We have removed the Resistance 470 and BAT54W, and tested the reset signal again, find that SBC reset signal is normal, the MCU reset signal is not correct. please see the attachment.

    For the reset circuit  how to modify it?

 

 

 

 

0 Kudos
Reply
9,185 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Could you please show me the signal waveform of TP0101 measured with an oscilloscope?
And please show the SBC circuit (including the RESET_SBC part)

0 Kudos
Reply
9,177 Views
asd046012
Contributor III

Hello

   The wave of reset signal measured by oscilloscope is as below.

    The signal RESET_SBC is input signal for the MCU,  and output by SBC,  so the reset signal is controlled by SBC.

 

 

 

 

 

reset.JPG

 

0 Kudos
Reply
9,199 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi asd046012,

Please refer the "5.2 RESET system" of AN5426, Hardware Design Guidelines for S32K1xx Microcontrollers

After flash program into the MCU, this phenomenon will no longer appear on the reset line.

5.2 RESET system AN5426.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply